Graphic Object Position

You can check the position and size of a graphic object using the graphic object position bar. The size and position is displayed in pixels.

If the objects are grouped together the position and size for the whole group is displayed. If you multi-select objects the position and size is displayed for all selected objects.

This feature is only available in Design mode.

For more information, see the Graphics User Interface Overview section.